This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC900: DLP9000

Part Number: DLPC900

Hi

Is it posible to Invert the data inputs in a Video mode as in a pattern mode?

We would like to place the DMD9000 in a 180º (new layout) and flip Image Short-Axis , the Front light is in the same location 

then we do not have mirror image but the display data is inverted (monomode) 

Thank you 

Arik

  • Hello Arik,

    Welcome back to the E2E forum. Thank you for your business!

    If you are using the DLPC900 dual controller EVM and the associated GUI, then within the System Settings panel of the GUI, the user can control the orientation of the image.

    The Dual Controller EVM East/West flip is permanently set to ON due to the dual controller implementation. Reverse pattern data in the images prior to loading or in the video data prior to loading or streaming video. 

    The North/South setting causes the image to be flipped on its short axis. This setting must be set before any Pattern LUT updates are sent to the DLPC900. The pattern sequence must be in the stopped state.

    Best,

    Maxine

  • Hello Maxine

    In video mode the North/South flip is working but the Pattern Display Invert Data has no impact on the display

    how can I invert the Data in a Video Mode?

    BR

    Arik

  • Hello Arik,

    Data is inverted through using the complement of each bit, i.e. 001->110. To verify, is this what you are trying to accomplish?

    Best,

    Maxine