This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710EVM-LC: How can I centre the projected image along the vertical axis

Part Number: DLP4710EVM-LC
Other Parts Discussed in Thread: DLPC3479, DLP3010EVM-LC

Hello Forum,

I am currently testing a setup with the projector and two cameras on each (left/right side), for the optical layout is convenient to have the height of the projected image centre along the horizontal and vertical axis. Nevertheless, according to the projector design this is not by default.

There is a way to modify the projection offset so the projected image can be aligned?

Regards,