Other Parts Discussed in Thread: DLPC900
Hi,
I am currently using a DLP6500FYE connected to the DLP Lightcrafter DLPC900 Evaluation Module. I would like to be able to precisely control the exact refresh rate of the DMD, the hope is that I i can expand a laser beam onto the DMD surface and cause the DMD to flicker from a complete in and off state so i can use that as a fast shutter. I have mechanical shutters that will go down to 20ms or 50Hz, but is there a way to control my DMD system in a similar way?
Say cause the DMD to show a white screen/ have all the mirrors "on" and then after 1ms turn all the mirrors to a black screen/ go to an "off" state? \
If there is anything I can add to help explain my question just let me know, also any info back is much appreciated!
All the best,
Dan Blackmore