Other Parts Discussed in Thread: DLP2010LC, DLP3010LC, DLPC3478
Dear TI experts,
My customer tests the modules with the combinations below ;
- DLPC3470(FW v7.3.1)+DLP2010LC
- DLPC3478(FW V8.0.1)+DLP3010LC
and we found that in Splash Pattern Mode, we can irradiate the light only monochrome, not RGB pattern.
1. Is it possible to irradiate RGB pattern sequentially after few monochrome splash pattern passed?
2. now my customer tests splash pattern to merge splash image and firmware binary using DLP firmware editor, and download to the device.
Is it possible to write(download) only splash pattern to the device, not merge to whole firmware binary?
If it can, what is the memory size for download splash image? Is it possible to download more than 1 splash image if the memory allows?
3. Does any customer use only splash pattern to operate DMD module? Can you provide the image sensor information and irradiating only monochrome or also RGB?
Best regards,
Chase