This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4620S-Q1: Sub-frame rate and comparison to the DLPC900

Part Number: DLP4620S-Q1
Other Parts Discussed in Thread: DLPC900, DLPC230-Q1, TPS99000-Q1

Hello experts

I have a couple of questions about the DLP4620SQ1 DMD:

1. The DMD needs to be driven by the DLPC230SQ1 controller - is this device capable of receiving arbitrary 1-bit frames (similarly to the DLPC900) and then displaying those at the upper limit of the 10kHz sub-frame rate?

2. Would it be possible to connect the DLP4620SQ1 via a custom interposer board so that it may be driven by the DLP5530SQ1 EVM kit, and would the software support this? If so, do you have examples of scripts that could be use to set up the board appropriately?

3. What synchronization signals are available from the DLP4620SQ1 (or the DLPC230SQ1) to synch the displayed subframe with the illumination?

Any help in this regard would be highly appreciated. Thank you in advance.

Kind regards,

Stuart