Other Parts Discussed in Thread: DLPA3005, , DLP4710, DLP4710EVM-LC, DLPC3438
Hi TI expert,
I encountered a problem with using firmware about FWSel_DLPC3439_DLPA3005_SeriesLED_pm2_i2c0x36_v7p7p1.img.I have a set of hardware that is working normally with firmware (FWSel_DLPC3439_DLPA3005_pm1_i2c0x36_v7p7p1.img),Now I want to use two LEDs to increase brightness,So I updated the firmware to FWSel_DLPC3439_DLPA3005_SeriesLED_pm2_i2c0x36_v7p7p1.img,replace a single LED with two LEDs connected in series,But the system is not working properly。Do these two firmware have any different requirements for the hardware system?
Thanks!