This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC7540: DLPC7540ZDC+DLP650TE

Part Number: DLPC7540


我们新做的7540的板子打板回来了,可以正常开机和显示logo,但是外部信号和test pattern显示不了,已排除edid的问题。
带dlp logo的splash和SFG的画面都可以显示,稍微复杂点的图片和外部信号(compser里面get sourc config出来的数据是正常的)就显示不了,这会是什么原因?
备注:我们的板子是10层板,原理图基本和开发板一致.