Dear Mayank-san,
I downloaded the DLPC3478 firmware from two locations:
www.ti.com/.../DLP3010EVM-LC
FIRMWARE
DLP3010EVM-LC-FW - DLP 3010 Light Control Firmware
www.ti.com/.../DLP-PICO-FW-SEL
FIRMWARE
DLP-PICO-FW-SEL-DLPC34XX - Firmware Selector for the DLPC34XX Controllers
Both versions are 9.0.1, but I noticed a difference in the release notes.
The difference lies in the range of exposure time.
For example, 8-bit monochrome in internal pattern mode:
up to 29012us or up to 6928us.
Is the maximum value 29012us?
Best Regards,
Kadowaki