This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710: how to adjust exposure time in internal mode through i2c protocol

Part Number: DLP4710
Other Parts Discussed in Thread: DLPC3479

I want to adjust the exposure time through i2c protocol in internal mode, but I cannot find the address of the register. Now I can only set the exposure time of the projector to project pattern in internal mode by loading the pattern and exposure time into flash. Can I adjust the exposure time without loading patterns into flash in internal mode? It would be better to control through i2c protocol.