This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCRC900DEVM: DLPLCR9000EVM cannot output video signal through external sources

Part Number: DLPLCRC900DEVM
Other Parts Discussed in Thread: DLPC900, DLP7000, DLPLCR70EVM, DLPC900REF-SW

Hi, I’ve bought a DLPLCR9000EVM, the DLPC9000 DMD and DLPC900 controllers. There’s no way to output video signals through external sources. In the video mode, all the sources work well except for Paraleled RGB. I’ve tried different GPUs (Nvidia and AMD) for both HDMI and DisplayPort. The EDID is detected by the computer, but none of these output any video signals. I’ve done the same thing on a DLPLCR70EVM (DLP7000 DMD evaluation board) with similar procedures, and it works perfectly. I’m wondering if this is a firmware or hardware issue.