Other Parts Discussed in Thread: MSP-FET,
Hello,
Could you kindly help me with the connection details from MSP-FET to EVM module.
Thank you
Kalaivani K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Could you kindly help me with the connection details from MSP-FET to EVM module.
Thank you
Kalaivani K
Hi Kalaivani,
Can you please say the purpose of using the MSP-FET? Do you want to reprogram and debug the MSP430?
Please note, the MSP430 is pre-programmed on the EVM. The MSP430 is not required or used when evaluating the EVM using the DLP Control Program GUI with the FTDI cable. The MSP430 is more so included to local demo purpose.
For the hardware connections to use MSP-FET with MSP430, you need to use jumper wire to connect the following pins between the MSP-FET and DLP2021LEQ1EVM:
MSP-FET | DLP2021LEQ1EVM |
Pin 9 (GND) |
J2 Pin 1 |
Pin 1- (TDO/TDI) |
J2 Pin 2 |
Pin 7 (TCK) |
J2 Pin 6 |
Regards,
Lori