Other Parts Discussed in Thread: DLPLCR67EVM, DLPLCRC900DEVM, , DLPC900, TPS65145, DLPR900
I was testing the DLPLCR67EVM kit with DLPLCRC900DEVM and the DMD isn't working (not showing images).
Currently, the DMD cannot properly show images. And I’ve been debugging that. I’ve been referring to the user manuals (DLP900 and DLP670S) and the TI online forum.
- Test USB, display port, power cables - correct
- Verify “Video Mode” configurations via manual - correct
- Verify “Video Pattern Mode” encoding schemes via user manual
- Verify “Video Pattern Mode” bit-depth dependent exposure time - correct
- Tested the voltage outputs of multiple pins on the DLP900 board - correct
- Verified the LED light outputs of multiple pins on the DLP900 board - correct
- Tested the voltage outputs of the DLP670S board - error
- There should be patterns showing on the DMD after the DLP900 board is powered on - error
I think the voltage output of the DLPLCR67EVM board is wrong. According to this post , you can test the VBIAS, VOFFSET, and VRESET testpoint of the DMD board. I tested it (connecting the ground to the ground of DLPLCRC900DEVM) and the voltage values doesn't match the DLP670S specsheet. The DLPLCRC900DEVM board test point voltages are working fine, so it's not a DLPLCRC900DEVM board problem.
Am I measuring the voltages correctly or is the DLPLCR67EVM board malfunctioninig?