This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP9000XUV: DMD for 325nm Laser Source

Part Number: DLP9000XUV

We are exploring the use of a DMD for laser patterning, and our chosen light source is a 325nm / 30mW laser.

As a result, we require a DMD that functions under the conditions of 325nm. Is it possible to proceed with placing an order for a DMD specifically designed to meet these specifications?

Additionally, it's crucial to note that our application does not require a wide spectral range.

Your insights and recommendations are highly appreciated. Thank you!