Other Parts Discussed in Thread: DLPA3000,
Hello Ti experts,
I have custom board with DLPC3478 and DLPA3000. I send commands to DLPC3478 to update internal pattern table via stm32. After i call project pattern (9Eh), it does not project patterns correctly (mostly projects only 1 pattern or no patttern). If i put 3ms delay between Write Pattern Order Table Entry and Write Internal Pattern Control, it projects patterns corretly. Is there a way to check Write Pattern Order Table Entry command processed and ready to project pattern signal? Is there a busy signal for command processing?
Best,
John