Dear TI,
we are considering the application of a DLP module to create a synthetic "slit" for a scientific prototype.
This expepriment will need to operate well below 365 nm so the protective glass in front of the array is a limitation.
Is it reasonable to operate a DLP array (of course in a cleanroom environment, maybe in a nitrogen flow) with the protective glass removed?
We think the alumiunum surface of the micromirrors will form an oxide layer when exposed to air, and this is compatible with having some reflectivity in the UV. Do you have any further details on this process?
Looking forward for your answer, kind regards,
Lorenzo