Other Parts Discussed in Thread: DLPLCR70EVM, DLPC410
Hi,
I am trying to run the pre-loaded test patterns. When powering on the board it gets stuck with D17 as green and D2 as red.
I am connecting the board to the DLPLCR70EVM via J13. I am using a 5V, 10A power supply. I made sure 5.0V was received at the J12 connector.
I made sure the proper voltages were present at TP9, TP21, TP10, TP3, TP25 and TP32 as specified in the Debugging FAQs here: https://e2e.ti.com/support/dlp-products-group/dlp/f/dlp-products-forum/1254555/faq-dlplcrc410evm-debugging-faqs
When I power the board, D3 turns on as green briefly before turning off and then D17 turns on as green. D2 turns on as red and stays on. No other LEDs on the board turn on after this.
J2 has all 5 jumpers in the 3.3V position. How do I know if this is correct?
In the Debugging FAQs document linked above it is suggested to reprogram the PROM as it may be corrupted, however the files for reprogramming cannot be found when clicking on the hyperlink in section 4.
Please advise next steps so I can display test patterns.
Thank you.