Other Parts Discussed in Thread: DLPA2005, , DLP300S
Hello,
I'm trying to make sense of the DLPC1438 way of controlling the light which uses dark frames and exposure frames and in general of the DLPC1438 + DLP300S + DLPA2005 combination.
The DLPC1438 has a maximum pattern rate of 60Hz both for binary and 8-bit patterns. Looking at the DLPC3479 documentation for reference, frames could be cut into multiple patterns as one frame is constituted of 24-bits. For example, one 24-bit frame could be cut into 3x 8-bit patterns.
In the case of the DLPC1438 as the patterns have a maximum rate of 60Hz, is it correct to assume that the minimum exposure time is 1/60 sec or 16.6 msec ? Or is one frame (1/60 sec) divided into exposure and dark frames (for example: Number of exposure frames = 1, Number of dark frames = 2 -> 33% of 1/60 sec ON and 66% of 1/60 sec OFF per 1/60 sec)?
Thank you for our help,
David