This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC200: 64-bit API Files

Part Number: DLPC200

Hello Team,

Posting on behalf of my customer:

Hi I am writing because a software package that we downloaded appears to be missing certain functions required by our instrument which is a Cel5500 DLP projector
It runs using some software packages made my Ti, specifically the DLPR200API
It was purchased from Digital Light Innovations (DLi)
We are needing to run this piece of equipment in a 64 bit LabView program, which requires a 64 bit version of two files, PortabilityLayer.dll and USBLib.dll.

This issue is the 64 bit version of these files downloaded from TI, are missing a few functions in the API, specifically the ones causing issues for us are the following:

DLP_PWM_Set Period
DLP_PWM_Set Cycle

These functions are present in the 32 bit versions of these packages.
Although the majority of SDK files were provided with the 64 bit download, the .cpp files weren't included, so we cannot simply add the functions manually and re-compile.

Additionally, since the 32 bit versions only provided the .dll, we don't have the required information to write these functions in. 
 
Regards,
Renan