Other Parts Discussed in Thread: DLPC7540, PCA9539, DLPA100, DLP650TE
Hello
We set up the purchased DLPC7540EVM and DPL650TEEVM according to the user guide.
I confirmed that I ran the Quick Start in Section 2 in order and completed up to 4.d in Section 2.4 and completed up to Figure 2-5.
However, LED D6 on the EVM board remains lit red.
What kind of signal is this?
Please tell me the solution.