Part Number: DLP2021LEQ1EVM
Other Parts Discussed in Thread: DLP3021LEQ1EVM, DLP3021-Q1, DLPC120-Q1
Tool/software:
Dear all. I have a few inquiries regarding DLP2021LEQ1EVM that I would like to ask:
1. According to the User Guide, it is mentioned that users can change the projection pattern by inputting the command through the DLP Control Program. The default setting plays a racing video, but when I followed the instructions in the User Guide and inputted the command , the display appeared to be abnormal.


2. I would like to know if the Sample Code downloaded from the provided link is the current factory code for the FLASH in the development version
https://www.ti.com/tool/download/DLPC153
3.If I understand correctly, to project a custom image, I need to program the FLASH using DLP Composer and then select the pattern using the DLP Control Program. Is my understanding correct?
4.Can the DLP2021LEQ1EVM only handle pre-stored images, or is it also capable of projecting in real-time?
Thank all~