The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP5530PROJQ1EVM: DLP5530PGUQ1EVM

Part Number: DLP5530PROJQ1EVM
Other Parts Discussed in Thread: DLP5530Q1EVM, DLP5533A-Q1

Tool/software:

Is there any parameter to change  to increase throw  distance to around 20ft

  • Hi Dubala,

    I'm sorry to inform you, but this is not possible with the projection optics that come with this EVM.

    This is taken from the DLP5530PROJQ1EVM's user's guide:

    The max throw distance is 635 mm.

    May I ask why you need a throw distance of 20 ft?

    Regards,
    Michael Ly

  • Hi Dubala,

    Are you considering an AR HUD type of application that would create a virtual image at 20 ft in front of the windscreen?  There are some optical designs that we can share that could achieve this type of application.  However, as Michael mentioned, the EVM itself is not cable to achieve this throw distance.  IT would require a new projection lens.

    Jason

  • Hi Michael,

    Our leadership wants to project some image like any logo at that distance. So could you please share any projection optics design that could be used with the DLP5530Q1EVM

  • Hi Jason,

    Actually the requirement of 20ft is not for AR HUD ,it is like for ground projection of any images ,warnings. could you please share any projection optics design that could be used with the DLP5530Q1EVM

  • Hi Dubala,

    One of my colleagues, Aishwarya, has sent you an email so that we may talk about this offline. Let's move there because there are multiple threads open.

    We think it would be good for us to communicate all these ideas via a single channel so we can work together as a team.

    Please reply to the email from Aishwarya when you get a chance. This will also allow us to share with you other design and project files in an easier way.

    Many thanks,
    Michael Ly

  • Vaishnavi,

    I think we have figured out a direction to go.

    To quote my email to you after our video call,

    • TI recommends you use the DLP5531LEQ1EVM, which comes with an optical engine
      • This evaluation module (EVM) is compatible with the higher-resolution DLP5533A-Q1 DMD
      • The EVM also has design files for you to view
      • The driver board (LED driver) has part number DLP5531Q1EVM, and you may also find this board’s design files on the product page linked above
    • We recommend you use the TI Automotive Control Program GUI in order to do your initial evaluations of the EVM, as it provides a python test suite that you may use as an IDE w/ debug available
      • The DLPC230 is the main IC, and you may find the programmer’s guide on the product page
      • This programmer’s guide also has an error code index for your debugging needs
    • We recommend you also look into TI's Adaptive Driver Beam (ADB) technology.

    If you have any issues along the way, please create a new E2E thread, and we will get back to you. Else, if you must share private information, you may send to my email or send a private message here on E2E.

    Thank you,
    Michael Ly