Hello Aaron,
Thank you very much.Another question,can we set Front end IC to display 4K+(3840*2400) by DLPC4420's IIC?
Tian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Tian,
I've split your question into a separate thread as this is not related to the past question.
The DLPC4420 EVM does come with a front-end board but this works with only supported chipset DMDs that produce 4K UHD devices - DLP780TE, DLP660TE, and DLP470TE.
It hasn't been tested to work with 4K+ resolution, consequently we don't currently have a 4K+ DMD EVM available for purchase. You are free to try it yourself with editing the EDID - support provided in the Software Package - or find another front-end solution. The 4K+ resolution is quite niche and may be under-supported.
Best,
Aaron