Tool/software:
Is there a Linux version of DLP Composer available?
Additionally, is there a command-line interface (CLI) version?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Is there a Linux version of DLP Composer available?
Additionally, is there a command-line interface (CLI) version?
Hi Hariom!
DLP Composer is Windows-only (though it *might* be able to be used on Linux via WINE. This has never been tested as far as I'm aware).
There is a CLI version. It's called `CLPComposer.Console.exe` and is located in the same directory as the main DLP Composer executable. It's quite simple in that it only takes a single argument; the path to a Composer project file (.dlpproj) and then builds that project. All project configuration must be done via the GUI.
Thanks!
Andrew
P.s., if you attempt to run DLP Composer via WINE please let me know the results!
Hi Andrew,
As per your suggestion, I attempted to run DLP Composer on Linux using WINE. The installation was successful, but the application crashed when I tried to import a project.
I've attached a snapshot of the error message, as well as the crash log for further analysis. Let me know if there's anything else I can try or if you have suggestions on how to troubleshoot this issue.

�DLPA�� d o w s \ s y s t e m 3 2 \ w m p . d l l �v߯�k�1�� �w��o��rM��(O �f�9DL��o��{���8J�2� r<>