Other Parts Discussed in Thread: DLPC900, , DLPC910
Tool/software:
Dear TI team and forum users,
I am looking for a small form factor DMD+Controller set that can display a live sequence of arbitrary binary patterns at kilohertz rate. The micromirror pitch needs to be 5.4 micrometers (or smaller) and the resolution at least 720p. (I posted a similar question about one year ago but did not find a suitable solution so far: e2e.ti.com/.../dlp4500-small-sized-dmd-solution-max-2-by-3-cm-for-fast-binary-pattern-generation-dlp4500-or-faster)
The models that I found so far (such as the DLP500YX in combination with the DLPC900 controller) are either limited in memory and do not allow a live sequence of binary images, or they receive live 8bit images and the decomposition into binary images is done internally (by the controller?), so that the content of each binary image can not be controlled by the user.
Please let me know if you have any information on systems that come close to the specifications written above.
Thank you very much and best regards,
Dorian