The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP2021LEQ1EVM: DLP2021LEQ1EVM

Part Number: DLP2021LEQ1EVM

Tool/software:

 I attempted to run DLP Composer on Linux using WINE. The installation was successful, but the application crashed when I tried to import a project.

I've attached a snapshot of the error message, as well as the crash log for further analysis. Let me know if there's anything else I can try or if you have suggestions on how to troubleshoot this issue.

4571.Crash_2024_09_19_09_05_31.log
�DLPA��dows\system32\wmp.dll�v߯�k�1��	�w��o��rM��(O �f�­9DL��o��{���8󂞚J�2� r<>K�j�>X�B�^���!�t�W�E�5iI𝐦��	�0��\]+!kC\���r�9�9_ sq ׳n	\iޥ6D�������}���n��9�d,�	�f�7�F;���
���<��cGn(��E�=�}�e�u�z��4�QK^݅S�֟H�_��M21'�\2��e�ϒ��L`�Vܰ톿T��Z:Rl�����_�3�b�L����H%�3j���:?z��U�Y�5�#n���(��1����Q{#{Lϫ��n�l`���.U˰���x����d�MU�T�D핾��=.�qޮ�Y�Ih�{�ws�h��l�@�d�w�lv	�H�~ȼ�:�� ӳA�Kk�k�Q��j�|BkU�go7<E��+@����P��������j�1�v��y	%̥y�(�4�(����>��U}A������,�<�@U�`��ԑ���V�!���e��997��e�р�@�wd��>		��&����0{ak���{��^�#�(?���l��� �x���}�C��v�m�^=��j���%(%��
Il"U��]��qu�hm�z
{"��-�=�\�>H��[.�@k�Ӳ̨R2+'MH��(��٥����Q�N��Ȍe�e3#�A����y���(��^8��4c���ȡ���B$i��n��Il�ܿ>�����&
*z���(OQ_�+���o����+
UbD�o������	Lt�[�#֟�¸f0m�bD�o���c�W���"m!�0�V?�����9L7�t>D��[2<^A����1��{��"Y�3!�`�F=���s<r�f�{�éDzI��^0��[j��p�[��H��$�C���2��x^�u��/ʅ%>Ν���1b�ء��򭕸t�>vKQ� 7a4��w\T�+:��ݴ]�K�6�r�����z	�
ɪS�NwR\nMF��L�����

  • Hello Hariom,

    Thank you for reaching out to us through E2E! I'm getting a member of our team to respond to you shortly.

    Best,

    Aaron

  • Hello Hariom,

    DLP Composer uses various other Windows utilities to function. See the decrypted snippet of the log you have sent below.

    9/19/2024 9:05:30 AM
    Exception : Unable to get the window handle for the 'AxWindowsMediaPlayer' control. Windowless ActiveX controls are not supported.
    Source : System.Windows.Forms
    TargetSite : Void EnsureWindowPresent()
    Stack Trace :
    at System.Windows.Forms.AxHost.EnsureWindowPresent () [0x00054] in <675fde255dd74577a7e2492386d6578e>:0
    at System.Windows.Forms.AxHost.InPlaceActivate () [0x0002c] in <675fde255dd74577a7e2492386d6578e>:0
    at System.Windows.Forms.AxHost.TransitionUpTo (System.Int32 state) [0x000d9] in <675fde255dd74577a7e2492386d6578e>:0
    at System.Windows.Forms.AxHost.CreateHandle () [0x00076] in <675fde255dd74577a7e2492386d6578e>:0
    at System.Windows.Forms.Control.CreateControl (System.Boolean fIgnoreVisible) [0x00045] in <675fde255dd74577a7e2492386d6578e>:0

    Unfortunately, it might not be possible to run DLP Composer on Unix OS.

    Thank you,

    With regards,
    Aishwarya

    **Edit**
    Hariom,

    Can you please try to enable ActiveX on your virtual machine? Also, have you tried to open an already imported project?

    Thank you,
    Aishwarya

  • Hi Aishwarya/Aaron,

    I was able to successfully run DLP Composer using WINE after installing a few ActiveX plugins.

    Are there any CLI commands available for rebuilding the image? I noticed a few applications like DLPComposer.Console and DLPComposer.FlashCompiler.Console.

    Could you provide any steps or guidance on how to use these for rebuilding?

    Thanks for your help!

  • Hello Hariom,

    That's great!

    Yes, you can use the CLI to build and rebuild project. The command format is as shown below:

    To build the project:
    DLPComposer.Console.exe <.dlpproj file path>

    To rebuild the project:
    DLPComposer.Console.exe <.dlpproj file path>  -r

    I am closing this ticket. Please create a new thread if you have any more questions.

    Thank you,

    With regards,
    Aishwarya