This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC6540: The spi communication between DLPC6540 and DLPA3005

Part Number: DLPC6540
Other Parts Discussed in Thread: DLPA3005, DLP471TP

Tool/software:

Our project design is based on DLPC6540+DLPA3005+DLP471TP. But we encounter a problem: when the main board power up, after DLPC6540 sends several spi commands  to DLPA3005, the INT_Z signal is immediately set low and the main board shutdown.

we use a logic analyzer to record the spi data, as the following picture shows:

But the register mapd in the datasheet of DLPA3005 shows only command address 00 ~ 08 (section 7.6). So we see that there are other command. We wonder what these comand means and what causes the INT_Z signal of DLPA3005.

Can anybody help? Thanks a lot!