Part Number: DLP6500FYE
Other Parts Discussed in Thread: DLP6500FLQ
Tool/software:
Hi,
we use DLP6500 to expose 8-bit patterns on photoresist using a 405nm laser.
DLP 6500 works in Video Pattern mode and the laser is controlled by the LED R output.
Unfortunately, the characteristics of each RGB channel are non-linear as shown in the figure below:

I made the measurement by displaying uniform gray boards, the integration time for each board was 100ms.
Pattern Mode settings: depth 8bit, start bit R0, exposure 4046us, dark time 0, Clear: RED, Frame change checked.
The visible depression and peaks in the characteristics are clearly visible in the exposures:
Displayed image (not exactly the same)
Irregular "rings" (light grey) can be seen in the exposure (the irregularity results from the additional application of a bitmap to equalize the lighting),
which result from the non-linear characteristics. They should not be visible.
We tried different Video Pattern Mode settings on different channels without any positive results.
What determines this behavior of the DLP6500 and how can it be fixed?