Part Number: DLPC350
Tool/software:
Hi,
When I double click on JTAG programmer icon for flashing the firmware into flash through DLPC350. I get following error. Output of sxstrace tool is also given here.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DLPC350
Tool/software:
Hi,
When I double click on JTAG programmer icon for flashing the firmware into flash through DLPC350. I get following error. Output of sxstrace tool is also given here.
Device name LAPTOP-D07JONQ5
Processor 12th Gen Intel(R) Core(TM) i5-1240P 1.70 GHz
Installed RAM 16.0 GB (15.7 GB usable)
System type 64-bit operating system, x64-based processor
Pen and touch No pen or touch input is available for this display
Edition Windows 11 Home Single Language
Version 23H2
Installed on 01-01-2024
OS build 22631.4317
Experience Windows Feature Experience Pack 1000.22700.1041.0
DLP LightCrafter 4500 JTAG Flash Programmer (Active) - Version 1.0 - 04/01/2014
Anish,
Also try the 2008 version. That is what most of these were written under, but 2010 should be compatible.
The unknown part here is that this may not work under Windows 11. We simply don't know considering these were written in the XP/Win 7 days.
Please let me know how it goes. It may also be possible to create a VM with Win 7. Not ideal, but as a stop gap.
Fizix,
Hello Anish,
It is not as simple as recompiling. Many of the libraries and other components were from the 2010 period and would have to be overhauled to compile specifically for Windows 11. I know that even for Windows 10 it took some work to get it to work with the older redistributables.
Run the sxstrace tool again and determine which libraries and versions are missing. I suspect the list will be smaller now.
Then search MS to see if there are installers in addition to the vcredist ones that can be installed to provide the missing ones.
This article may be helpful: https://www.veritas.com/support/en_US/article.100039044
Fizix