Part Number: DLPC1438
Other Parts Discussed in Thread: DLPA3005,
Tool/software:
Hi
I have a board with DLPC1438 and DLPA3005.The problem is that after setting the PROJ_On signal to high, the HOST_IRQ signal stays high. The DMD cable and LEDs are connected.
1.I have checked the power-up Timing signal:
PROJ_On->VDD-1.1V、VCC18-1.8V、VCC_INTF-1.8V、VCC_FLSH are always 3.3V when SYSPWR is on.
PARKZ is 1.8V when SYSPWR is on,and go 3.3V when PROJ_On.
FPGA PWR go high.PLL_REFCLK 24MHZ stable.
RESETZ is 0.5V when SYSPWR is on,and go 1.8V when PROJ_On.
FPGA_RDY go high earlier then Host_IRQ.
Host_IRQ stay high.
VOFS=10V、VBIAS=18V、VRST=-14
what else singal should i check.
2.I have observe another situation.When the board is in normal temperature(about 28~30C).Host_IRQ will stay high after Proj_on.If i use heater to heat up the DLPC1438 to about 50C.Host_IRQ can go low in 2sec.Do you have any idea about this situation.