This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP2000: Using DLP2000 or DLP650LE with a pulsed laser

Part Number: DLP2000
Other Parts Discussed in Thread: DLP650LE, DLP160CP, DLP650LNIR, DLP4500NIR, DLPDLCR2000EVM, DLP4621-Q1

Tool/software:

I have been evaluating either DMD in an experiment incorporating a DLP2000 or DLP650LE on a torsion pendulum inside a vacuum chamber ranging in 10^-6 Torr. I am evaluating a pulsed laser source of a 3W 520nm or a 5W 980nm. I want to drive the torsion pendulum with the pulsed laser at approximately 8 Hz, so I must identify the corresponding duty cycle. This experiment will resemble the apparatus outlined in "Characterization for a Sensitive Inverted Pendulum Thrust Stand for Pulsed Propulsion with Optical Heterodyne Sensor and Lock-in Detection" by K. Chandrasekar et al. 

I started with your document DLPA027B, "Digital Micromirror Device Thermal Considerations Including Pulsed Optical Sources," but it does not appear compatible with the Pico DMD family. I would like to understand what I need to evaluate differently with the Pico DMD family. 

Here is my attempt to follow DLPA027B with the DLP2000 (DLPS140B) using a 3W 520nm laser:

  1. Mirror Surface to Bulk Mirror Delta
    1. q=95.49 W/cm^2
      1. focused on a 2mm diameter area at the center of the DMD
    2. q_adjusted = q*(1-MR) = 5.73 W/cm²
      1. MR=0.89 at 520nm (from DLPA027B)
    3. deltaT_Mirror Surface to Bulk Mirror = 2*q_adjusted*(1/k) sqrt((alpha*t_pulse)/π)+T_i = 20.3 C
      1. k=160 W/(m-C) (from DLPA027B)
      2. alpha=6.47E-5 m^2/s (from DLPA027B)
      3. t_pulse = 2.5ms
      4. T_i=20 ºC (assumed starting ambient temperature)
  2. Bulk Mirror to Silicon Delta
    1. Q_incidident mirror = q * pitch² = 5.46E-5 W 
    2. Q_mirror = Q_incident mirror * (FF_on*(1-MR)) = 5.59E-6 W
      1. FF_on = 0.931 (from DLPA027B)
      2. MR=0.89 at 520nm (from DLPA027B)
    3. T_f  =  T_i + (Q_mirror * R_mirror to silicon) = 22.5 ºC
      1. T_i=20 C (assumed starting ambient temperature for initial pulse)
      2. R_mirror to silicon = 4.47E5 ºC/W (from DLPA027B not in DLPS140B)
    4. T_off = 0.1225s >> 5τ [fully cools]
      1. τ=11.49μs (from DLPA027B)
    5. deltaT_Bulk Mirror to Silicon = T_f + (T_i + T_f) e^(-t_pulse/τ) = 22.5 ºC
      1. T_i=20 ºC (assumed starting ambient temperature for initial pulse)
  3. Silicon to Ceramic Delta
    1. Q_electrical = 0.045 W (from DLPS140B example)
    2. α_DMD = (1 - Overfill) *((FF_off * (1 - MR)) + (1 - FF_off)) + (2 * α_window) + Overfill = -4.99 <= This seems wrong
      1. FF_off = 0.724 (from DLPA027B)
      2. MR=0.89 at 520nm (from DLPA027B)
      3. α_window = 0.007 (from DLPA027B and cross-referenced with DLPA031E)
      4. overfill = 1 - (Active Array Area/Incident area) = -17.6 <= This seems wrong
        1. Active Array Area = (7.57μm * 1280) + (7.57μm * 800) = 5.85E-5 m²
        2. Incident Area = 0.25 π d^2 =3.142 d²  = 3.14E-6 m²
          1. d = 2mm (assumed projection area)
          2. I do not intend to project onto the entire DMD, as the pendulum will oscillate along the DMD width. 
          3. I believe that the overfill is intended to reflect how much light is incident onto the ceramic. 
    3. duty cycle = t_pulse/(t_pulse+t_off) = 0.02
      1. t_pulse = 2.5ms
      2. t_off = 0.1225s
    4. q_average optical power density = q * duty cycle = 1.91 W/cm²
    5. q_average optical power = active area area * q_average optical power density = 1.12 W
    6. Q_illimunation = α_window / q_average optical power = -12.3 W <= This seems wrong
    7. deltaT_Silicon to Ceramic = (Q_electrical + Q_illumination) * R_Silicon to Ceramic = -6.12 ºC <= This seems wrong
      1. R_Silicon to Ceramic = 0.5 ºC/W (from DLPA027B, not in DLPS140B)
  4. Mirror Surface to Ceramic
    1. T_mirror surface = T_ceramic + deltaT_Mirror Surface to Bulk Mirror + deltaT_Bulk Mirror to Silicon + deltaT_Silicon to Ceramic = 56.68 ºC

A few related questions: 

  1. In Section 6.5, the DLP2000 and DLP160CP each provide only the Thermal Resistance as measured at TP1. Why not also provide the R_mirror to silicon and R_Silicon to Ceramic? 
  2. The DLP160CP provides a small area for a thermal interface, but the DLP2000 does not. Is there any documentation on the thermal interface for the DLP2000 ribbon? 
  3. Above 800 nm, both DMDs are limited to 10 mW/cm^2; however, does this not depend on the duty cycle? I am asking this to understand if the 5W 980nm laser I have available will be a useful substitute. 

  • Hello User,

    Welcome back to the E2E forums and we hope to assist you with your questions.

    Please give our team some time to check internally and will get back to you when I find more information.

    Regards,

    Alex Chan

  • Hello User,

    Please see the responses from the team in red. 

    1. Mirror Surface to Bulk Mirror Delta
      1. q=95.49 W/cm^2
        1. focused on a 2mm diameter area at the center of the DMD
      2. q_adjusted = q*(1-MR) = 5.73 W/cm² (this assumes MR = 0.94, at 520 nm MR = 0.89 and q_adjusted = 10.5 W/cm^2)
        1. MR=0.89 at 520nm (from DLPA027B)
      3. deltaT_Mirror Surface to Bulk Mirror = 2*q_adjusted*(1/k) sqrt((alpha*t_pulse)/π)+T_i = 20.3 C deltaT_Mirror Surface to Bulk Mirror = 2*10.5 W/cm^2 *(100^2 cm^2 / 1 m^2)*(1/160 W/m-K)* sqrt((6.47e-5 m^2/s*[2.5 ms * (1s / 1000 ms)]/ π)+ 0 = 0.3 ºC

    *The mirror surface to bulk temperature rise is quite small in this case

    1. k=160 W/(m-C) (from DLPA027B)
    2. alpha=6.47E-5 m^2/s (from DLPA027B)
    3. t_pulse = 2.5ms
    4. T_i=20 ºC (assumed starting ambient temperature) The mirror temperature rise above the bulk is just 0.3 ºC.  If the bulk mirror is 20ºC, then the surface is 20.3 ºC

     

    1. Bulk Mirror to Silicon Delta
      1. Q_incidident mirror = q * pitch² = 5.46E-5 W 
      2. Q_mirror = Q_incident mirror * (FF_on*(1-MR)) = 5.59E-6 W
        1. FF_on = 0.931 (from DLPA027B)
        2. MR=0.89 at 520nm (from DLPA027B)
      3. T_f  =  T_i + (Q_mirror * R_mirror to silicon) = 22.5 ºC
        1. T_i=20 C (assumed starting ambient temperature for initial pulse)
        2. R_mirror to silicon = 4.47E5 ºC/W (from DLPA027B not in DLPS140B)
      4. T_off = 0.1225s >> 5τ [fully cools]
        1. τ=11.49μs (from DLPA027B)
      5. deltaT_Bulk Mirror to Silicon = T_f + (T_i + T_f) e^(-t_pulse/τ) = 22.5 ºC
        1. T_i=20 ºC (assumed starting ambient temperature for initial pulse)

    Calculation is correct.  The bulk mirror temperature rise above the silicon is just 2.5 ºC. 

    1. Silicon to Ceramic Delta
      1. Q_electrical = 0.045 W (from DLPS140B example)
      2. α_DMD = (1 - Overfill) *((FF_off * (1 - MR)) + (1 - FF_off)) + (2 * α_window) + Overfill = -4.99 <= This seems wrong

    This calculation assumes the entire array is illuminated or it possibly even has overfill outside of the active array.  If the illumination spot is entirely within the active array, simply assume overfill = 0.  Then α_DMD = 0.36964.  This is the absorptivity of the mirrored array plus bulk window absorption.

    1. FF_off = 0.724 (from DLPA027B)
    2. MR=0.89 at 520nm (from DLPA027B)
    3. α_window = 0.007 (from DLPA027B and cross-referenced with DLPA031E)
    4. overfill = 1 - (Active Array Area/Incident area) = -17.6 <= This seems wrong (just assume overfill = 0 for the underfilled array case)
      1. Active Array Area = (7.57μm * 1280) + (7.57μm * 800) = 5.85E-5 m² (DLP2000 is a 640 x 360 array with 7.56 um pixel, DLP650LE is a 1280 x 800 array with a 10.8 um pixel. Just choose one or the other for this calculation.)
      2. Incident Area = 0.25 π d^2 =3.142 d²  = 3.14E-6 m²
        1. d = 2mm (assumed projection area)
        2. I do not intend to project onto the entire DMD, as the pendulum will oscillate along the DMD width. 
    • I believe that the overfill is intended to reflect how much light is incident onto the ceramic. 
    1. duty cycle = t_pulse/(t_pulse+t_off) = 0.02
      1. t_pulse = 2.5ms
      2. t_off = 0.1225s
    2. q_average optical power density = q * duty cycle = 1.91 W/cm²
    3. q_average optical power = active area area * q_average optical power density = 1.12 W (This should be average power density * illumination area for your case, so 1.91 W/cm^2 * 3.14E-6 m² = 0.06W)
    4. Q_illimunation = α_window / q_average optical power = -12.3 W <= This seems wrong (This should be α_DMD * Q_incident = 0.36964 * 0.06W = 0.022W)
    5. deltaT_Silicon to Ceramic = (Q_electrical + Q_illumination) * R_Silicon to Ceramic = -6.12 ºC <= This seems wrong (delta_T_Silicon to Ceramic = (0.045W + 0.022W) * 8ºC/W = 0.54ºC
      1. R_Silicon to Ceramic = 0.5 ºC/W (from DLPA027B, not in DLPS140B) (Technically we should generate a new R_Silicon to Ceramic from a package thermal model since the value will be higher because we have all the heat load in a small spot size. Note: DLP2000 is 8ºC/W with full array illumination.  The 2 mm spot covers about 24% of the array.  Even if the package resistance increased to 16 ºC/W, the temperature rise would be ~1ºC.  Electrical load is spread over the entire area so the effect would be less than this, so 1ºC is probably worst case.)
    6. Mirror Surface to Ceramic
      1. T_mirror surface = T_ceramic + deltaT_Mirror Surface to Bulk Mirror + deltaT_Bulk Mirror to Silicon + deltaT_Silicon to Ceramic = 56.68 ºC

    (This should be T_mirror_surface = 20ºC  + 0.3ºC + 2.5ºC + 1ºC = 23.8ºC.)

     

    A few related questions: 

    1. In Section 6.5, the DLP2000 and DLP160CP each provide only the Thermal Resistance as measured at TP1. Why not also provide the R_mirror to silicon and R_Silicon to Ceramic? (Mirror to silicon temperature rise is only significant with pulsed sources. Most of our applications use continuous sources.  R_silicon-to-ceramic is the same as thermal resistance as measured at TP1 since TP1 is on the ceramic)
    2. The DLP160CP provides a small area for a thermal interface, but the DLP2000 does not. Is there any documentation on the thermal interface for the DLP2000 ribbon? (The DLP2000 is intended for low power applications and therefore does not have a dedicated thermal interface area)
    3. Above 800 nm, both DMDs are limited to 10 mW/cm^2; however, does this not depend on the duty cycle? I am asking this to understand if the 5W 980nm laser I have available will be a useful substitute. (These DMDs were intended for visible applications and therefore were not tested above 800 nm. TI offers several DMDs intended for IR applications such as the DLP4500NIR and DLP650LNIR)

    Regards,

    Alex Chan

  • Alex and Team, 

    Thank you for your response, and my apologies for the MR errors that were transferred from me working through your examples. I understand that the DLP2000 is ideal for low power applications, however, given its size it might be my best option for the small moment of inertia in my experiment. A few more questions and I should be good for a bit: 

    1. Do you have any guidance on thermal conductivity from the DLP2000 into the Panasonic AXT542124DD1 socket? I assume that was done when designing the DLPDLCR2000EVM. 

    2. The DLP4621-Q1 appears to be a better DMD for this application; however, given its size (and assumed weight) and much larger power requirements, I am dissuaded from considering it. Do you know of a lightweight DMD with good thermal transfer properties and low power requirements? 

    Thank you. 

    Jonathan

  • Hello User,

    Let me check futher with the thermal team and will get back to you.

    Regards,

    Alex Chan