Part Number: DLPC3478
Other Parts Discussed in Thread: DLP3010, , DLPA2005
Tool/software:
Hello.
I am using DLPC3478+DLPA2005+DLP3010.
(F/W Version 9.0.1)
So far, the development has been completed without any special issues and is currently in mass production.
I would like to thank the TI staff who have helped me so far.
There is something I would like to test additionally.
I would like to output the RGB image below as a Splash pattern or in another way.

Is there a method you can recommend?
Every time a pattern is output, a trigger should be generated through Trigger1 or Trigger2.
It is okay if the pattern output time is slow.
I have tested it through Splash pattern so far, but it is only output in a single color.
Please reply.