Part Number: DLPC3432
Other Parts Discussed in Thread: USB2ANY
Tool/software:
Dear TI engineer,
Our projection occasionally appears the problem of flower screen and stuck in the first frame, help to see how to analyze this problem,tks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello user,
Please provide the firmware version you are using and the steps you've been went through to see the issue.
Regards,
Lori
Hello,
Looks like you are using v7.4.2. Can you please confirm if any changes have been made to the firmware? Could you also provide a detailed description of the issue? If you are referring to the black and white vertical bar issue, this is usually causes when in external video mode without providing some time of video data.
Please also see our hardware diagnostic tool to help debug (TI DLP Pico Hardware Diagnostic Tool).
Best,
Max
Hello,
Did you fill out the export control form it asks before downloading? Can you also please provide the previously requested details?
Best,
Max
Yes, I did. Mostly names, companies and military entities.I just got customer service working on it.
Hello,
I need details regarding the issue that is being reported, please describe what issue you are facing and the steps to reproduce it.
Best,
Max
Hello,
I think there might be some confusion, I am referring to the issue originally reported with the DLP system.
Best,
Max
Our projection occasionally appears the problem of flower screen and stuck in the first frame.
Please provide the steps/commands you send to setup the video and reproduce this issue.
Best,
Max
Hello Maximus,
ok,I'll send it to the office tomorrow.
I downloaded it now TI DLP Pico Hardware Diagnostic Tool.
What tool do I need to connect my hardware diagnostic tool to DLP technology controller, i2c to usb tool?
SCL, SDA, 3.3V and GND pins Which pins to connect to DLPC3432?

Hello,
Please see our guide on DSI setup and debugging. Additionally please ensure via your hardware that DSI data lanes remain in spec during video transmission according the DLPC3432 datasheet.
Best,
Max
Hello,
We are configured according to this file, and now the probabilistic flower screen, how can I reverse prove that there is a problem with my previous DSI setting.
Hello,
We are not DSI experts, all I can suggest is ensuring the DLPC DSI spec is followed and setup according to the guides I have provided you. Do you have any additional information on when this behavior is observed? Do you ever see a stable/clean image via DSI?
Best,
Max