Tool/software:
Hello,
I am right now working with a DLP650LNIR for my master thesis. Because we want to use the DMD later to influency atoms in a MOT, we want the output to be as stable as possible. I realised, when looking at the DMD output with a photodiode, that there seems to be a flickering effect for the mirrors dependent on the illumination/picture time. I think this is to prevent the mirrors from getting stuck in one position, when a picture is portrayed for a long time. For our use, the DMD will just be active for around 1 minute. So this setting should be disabled, but I'm not sure if thats possible with the API or the hardware settings.
Here is a picture for reference: