Hello,
I'm programming the APPSFPGA to interface with an external A2D board with an operating supply between 2.7V - 5.5V. I'm interested to use the J6 GPIO connector for the interface with a power supply of 3.3V.
The reference manual (2510455) says that it is a 2.5V connector, which is indeed what I see on the example FPGA code supplied by TI. However, I was wondering if there is a reason why I should avoid reprogramming the corresponding virtex5 pins to 3.3V?
Thanks.