This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How could I project in this mode?



Hi:

Recently, I wanted to use a camera and  LightCrafter to build a three-dimensional measurement system.Cameras and LightCrafter coordination process is as follows:

1、I have upload 7 images to LightCrafter,and select the stored pattern sequence.

2、I connect PIN3 of J7 to camera's trigger,and I have set the output trigger enable.

3、I wish the LightCrafter project the first image and then trigger the camera to taking one picture. Then project the second image and trigger the the camera to taking the second picture............At last,the LightCrafter project the seventh image and trigger the camera taking the seventh picture. Then the LightCrafter stops projecting image  3 seconds and then start from the first image.........Cycle work!! I hope  the LightCrafter project the first to the seventh image as soon as possible,much less than 3s.

Thanks a lot!

Lijianglong