Hi,
I have a question about the temperature measurement by the combination of DLPA2005/DLPA3000 and DLPC3438.
I'd like to change the thermistor from the EVM reference to other parts.
Reference NCP15WF104F03RC(Murata) → For example,NTCG104LH104(TDK)
Is it possible to change the settings in the LightCrafter Display 3010 EVM GUI?
Is it can be adjusted by changing the fixed resistance value, such as R22.
or should I use the MURATA of reference?
Best regards,
Seishin