Hello,
I would like to use the DLP6500FYE in combinatio with a near infrared tunable laser light source.
I therefore have a few questions:
1) Is there any problem with the functionality of the device within the near infrared region?
2) Is the glass window anti-reflectivly coated?
If yes, is the coating still fine within the wavelength range of 820nm to 890nm?
3) Is there an issue with interference effects due to the application of a coherent light source?
Many thanks in advance!