I am trying to turn on my dlp light crafter 6500 evm for the first time and I get no power on light or connection to the software interface. I am using the 6 pin molex connecter to an ATX powersupply. I have verified that the plug is putting out 12 VDC with a multimeter and that the positive and negative terminals at the power plug are getting 12 V on the board but still nothing. Am I missing something or should there be something else that I should try? Please advise.
Thanks,
Michael