Support,
I have a problem connecting to the TIDA-00293 DLP device
http://www.ti.com/tool/tida-00293
via a standard USB cable and D2XX drivers.
I have followed this installation guide
https://dl.dropboxusercontent.com/u/48163342/dlpu025.pdf
First I have installed the D2XX drivers using windows setup, which indicated the successfull installation.
I was able to connect to the device using DLP LightCrafter 4500 Control Software, uploaded the new firmware and was able to manipulate the LEDs.
However I am not capable to connect to this device using the D2XX driver, which is necessary for programming it: neither with the DLP_3D_Printer software provided by the TI, nor using the Software Development Kit (SDK) examples. The error I get is that FTD2XX.dll is missing, which indicates to the issue with the driver. As a matter of fact, the SerialPort converter does not appear in the Device Manager. It is recognized as HID in the Devices and Printers (see screenshot). When I tried to update the driver the Windows left the same one stating that this is the most current driver. I have tried this procedure on different operating systems: Windows 10 x64, Windows 7 x86, and Windows XP x64 with the same result, even with the signed driver check set to OFF. I start to suspect that USB cable is not meant to control this device using D2XX drivers.
Could you please enlighten me, what could be the issue behind this problem? Should I just use a different cable, which one is the recommended then? Otherwise I would prefer using the present cable because of the timing-reasons.
Thanks for any help.