Hi,
I have a question on DLP9000XFLS. It seems that the device can operate up to approximately 15 kHz whereas DLP9000FLS can operate only up to 9.5 kHz. What is the main difference between the associated drivers?
Also, for the DLP7000 and DLP9500 chips there are high speed operation solutions available from some of the partner companies of TI such as Digital Light Innovations and these systems are generally based on an on board memory units. Is there a similar unit on the driving board of DLP9000FLS and DLP9000XFLS, if so how many binary patterns can be stored inside these units?
Thank you.