Hello to whom it may concern,
Could you please teach about flash memory of DLPC200?
1, Could you pleas teach required specification of parallel NOR flash memory for DLPC200?
I'd like to know the required memory size or speed grade etc.
2, Can we use below flash memory for DLPC200?
a, MT28EW01GABA1HPC-0SIT(Micron)
b, S29GL01GS series(Cypress)
If we can't use above memory,could you please teach recommend flash memory of BGA type?
Because the availability of recommended parallel flash memory(JS28F00AP30BF) is bad, so we want to know.
Best regards,
Manabu Ito