The host only communicates with the DLP chip set over the I2C bus to the DLPC150 controller. However, the DLPC150 picks up the DLPA registers via its SPI_1 port. So how does the host read & write the DLPA registers? I do not see commands to do this in the DLPC150 Programmer's Guide.