This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC200: DownloadBPPfromFlashToExtMem(0x0030) command via SPI does not display expected image

Guru 10570 points
Part Number: DLPC200



Hello.

I have a question about DownloadBPPfromFlashToExtMem(0x0030) command of DLPC200.


When I send the command via SPI, the expected image does not display.
Do you have any advice to display image appropriately via SPI?


Case-a) I am sending following command via SPI and Write Resp returned with no error.
Tx Command: 02AA0000 0C00 3000 0000 00000400 00800100 (WriteResp : 03AA0000 0200 0000 02)
(This command was generated by LightCommander Log "DLP_Img_DownloadBitplanePatternFromFlashToExtMem 0x00040000, 98304, 0")

Case-b) When I send via USB by LightCommander GUI "Command Line Window", Light commander works as expected.

Best regards, RY