This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC910: TIDA-00570 High Speed DLP Sub-system DLPC910 Main Board

Part Number: DLPC910
Other Parts Discussed in Thread: TIDA-00570,

In the schematic of Evaluation kit "TIDA-00570 High Speed DLP Sub-system DLPC910 Main Board" drawing № 2514435 there are some pins used at DLPC910, which in Datasheet are classified as "Reserved" pins.

I would like to know if I really need these pins to connect for proper operation or I can simply ignore them..?

These pins are: AC12, AD11, AA9, Y10, Y11, AB11, F8 (p.9 and p.11 of schematic 2514435)