Other Parts Discussed in Thread: DLP5500,
Dear,
I've made application board using DLPC200 and DLP5500.
working is good so far but some question as below picture is screen shot in LVDS Clock of DLP5500 board. but duty cycle is different as i marked "A", "B".
i think since it is clock signal, it must be fixed but marking A is longer than marking B. i have to verify it is normal signal or there are some problem.
because i have to prepare mass production using this device.
please help it is normal signal or not.
if you can't check below picture, please check attached the file.
thanks.