This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPA200: DLPA 200 PFC could not be found.

Part Number: DLPA200


Hi,

I can not find the DLPA 200 PFC.

Is DLPA 200PFP the successor product? Is there compatibility?

I would be pleased if you give me advice.

Best Regards,

Leonardo

  • Hello Leonardo,

    If you are looking for the DLPA200 DMD Micromirror Driver, the current orderable part number is indeed DLPA200PFP.  

    As far as I know this is the only part number.   Where did the "PFC" come from?  Maybe it is a typo.

    Fizix

  • Hello Fizix,

    I found DLPA 200 PFC on 2 pages of DLPA 200 data sheet.
    I would appreciate it if you could refer to the following.

    Changes from Revision B (August 2012) to Revision C Page
    • Added DLPR4101 to DLPR410 througout document............................................................................................................. 4
    • Changed DAD2000 to DLPA200 in the Serial Communications Port (SCP) section........................................................... 17
    • Changed text From: DLPA200PFC is functionally. equivalent.. To: DLPA200PFP ............................................................ 22

    Best Regards,
    Leonardo
  • Hello Leonardo,

    I think I understand the confusion now.  The note:

    Changed text From: DLPA200PFC is functionally. equivalent.. To: DLPA200PFP ............................................................ 22

    Is noting that DLPA200PFC appeared in the previous version (it was a typo), and was corrected.  In other words the text was changed from the erroneous DLPA200PFC to the correct DLPA200PFP.

    I hope that helps.

    Fizix