This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What is the flux-density damage threshold of DMD's?

Other Parts Discussed in Thread: DLP5500

Hello

What is the highest flux density damage threshold available for DMD chips, and which product has the highest damage threshold?

I am considering the possibility of using DMD's for a rather high-power application. It is in this context, that my question on damage threshold arises.

The light source could be either a broadband light source or a laser light source.

I need to do a spatial light modulation of about 3 kW of CW-power. Can this be done with only 1 DMD or should it be divided up onto several? In the latter case - how many DMD's would be needed?

Grateful for any advice you may be able to provide.

Regards, David