Other Parts Discussed in Thread: DLPC3439
Hello,
1. In DPP343x_software guid.pdf, i find these register address, C0 & D6, what the function is? and which one i can read to know DLPA3000 temperature?
2. Write the 0xC0 (register address) and 0x00 (read parameter), and then read two bytes of data
Issue:
When the fan is not used blows the chip, the data read will be reduced every time the operation is performed until the reading value is 0.
When the fan blows the chip, the data read from each operation is increased until the reading value is around 0x02,0xee.
any wrong for the procedure? or what is the correct solution?
3. How to set the DLPA3000 UVLO, or can i use DPP343x control DLPA3000 UVLO?
thanks!