Hi Kyle,
One more question:
I found that we can use the solution to save the configuration (store pattern sequence) and the image into the lightcrafter, then set the solution as default. This able to solve the problem and no GUI needed when my application is running. But it having an issue which is the image sequence cannot be reset. As i know we only can use the IO to trigger next image. If there have miss trigger IO will cause the sequence inaccurate. I know that if using the GUI when press the stop and start button the sequence will reset. If there any other method to reset without using the GUI?
Thanks,
Lee SW