Other Parts Discussed in Thread: TIDA-00361, DLPDLCR2000EVM, DLPC2607
Hello,
There arew two thing that I want to do, the first one is as the question states, how can I run DLP2000 (the one that is a beaglebone cape) run on Raspberry Pi and Windows IoT? I've read that it is possible, but I haven't found much information on people actually doing it.
The reason for using windows 10 IoT, is that I want to do something similar with the DLP2000 as the TIDA-00361. I want to use this projector in order to obtain a point cloud. With the DLP3000 EVK is simple because the SDK already supports it, but there is no built-in support for DLP2000. Is Texas Instruments planning on adding the DLP2000 projector to the SDK or will I have to do it on my own? If so, is there any available documentation that could assist me on doing it?